250929_LSS100100/LSS100200_SW_03.0

Factory Reset

The factory reset feature erases all configurations and restores the device to its factory default settings, while leaving the system settings unchanged.

Software factory reset

The software factory reset, which can be initiated from the main menu, does not change the IP address. It performs the following actions:

  • Erases visualization, applications, graphics, and all data.

  • Resets the device name to the default (SpaceLYnk/Wiser for KNX).

  • Resets the KNX settings to default.

  • Deletes FTP and Nginx certificates.

  • Sets the FTP password to empty.

  • Deletes Lua scripts, including planned and init commission.

To reset the IP address to the default (192.168.0.10) while preserving the project, press the HW reset button for 10 seconds. This feature is helpful if you’ve forgotten or incorrectly set the IP address.


Hardware factory reset

The factory reset with the hardware button is particularly useful in situations where the controller is inaccessible due to incorrect settings.

To perform a hardware (HW) factory reset, locate the RESET button on the front side of the controller. Press and hold this button for 10 seconds, release it, and then press and hold it again for another 10 seconds.

After a HW factory reset, the IP address will always be reset to 192.168.0.10.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?