250929_LSS100100/LSS100200_SW_03.0

Direct Link

The Direct link icon at the bottom left opens a dialog to create a direct link for the scheduler visualization. This link can include the IP address of the host and specify whether to display holidays in the scheduler.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?