Adding Sequences to Scenes
Adding a sequence to a Scene
-
Click Add objects to add objects and status objects to create your sequence. You can take live values from either the status object or the main object. Additionally, you have the option to specify a delay before writing each sequence.
-
The other following actions are available:
-
Run scene: Instantly execute the scene.
-
Save live values: Save the actual values of objects within the scene.
-
Change sort order: Use drag-and-drop to reorder the sequence in scenes.
-
Delete: Remove a sequence.
-
-
To manually set the value of an object, click
in the Set value column of the Sequence for scene dialog. -
You can sort the order of objects within the scene using the Move up and Move down arrows, or delete them as needed.