250929_LSS100100/LSS100200_SW_03.0

Date and Time

The controller implements the Network Time Protocol (NTP). With an internet connection, controller automatically updates the time from the servers defined in Utilities/Services/NTP Client/Server:

  • 0.schneider.pool.ntp.org

  • 1.schneider.pool.ntp.org

  • 2.schneider.pool.ntp.org

  • 3.schneider.pool.ntp.org

Timezone: It is crucial to select the correct time zone.

Get from system: If there is no internet connection, click on Get from system to adopt the time from your PC.

First day of the week: You can select the starting day of the week according to your preference.

Latitude/Longitude: Set up the latitude and longitude coordinates of the geographic position of the controller for accurate calculation of sunrise and sunset times. If not set, these times are calculated from the time zone, which may result in inaccuracies.

The exact geographic position can be easily found on Google Maps by right-clicking on your location on the map.


NOTE: Without power, the controller will maintain time and date settings only for a limited time (approximately 5 minutes).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?