2410_LSS100100/LSS100200_SW_03.0

Introduction

This document outlines the features and programming interface for the spaceLYnk and Wiser for KNX controllers (referred to as the “controller”).

The software programming interface is integrated within the controller and can be accessed via a web browser.

It is essential to note that pre-programming and configuration tasks are only possible with the controller. Before proceeding with installation, operation, or maintenance, carefully review the instructions and become acquainted with the device

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?