250929_LSS100100/LSS100200_SW_03.0

EnOcean USB Gateway

  • Compatibility:
    The controller EnOcean functions have been thoroughly tested with the EnOcean USB Gateway LSS10020040. Keep in mind that this specific product reference may not be available in all countries. However, any USB EnOcean gateway based on the EnOcean organization USB 300 (OEM) product can be used by third parties.

  • Frequency considerations:
    EnOcean operates on different frequencies depending on the geographical region:

    • 868 MHz: Europe

    • 902 MHz: USA/Canada
    • 928 MHz: Japan
    • 2.4 GHz: worldwide usage
  • The EnOcean USB gateway is a compact USB stick that connects various devices (PCs, consumer devices, DSL boxes) to EnOcean-based radio products.

  • Equipped with a TCM 310 transceiver gateway module, it provides bidirectional EnOcean radio communication and a bidirectional serial interface via USB.

  • Radio messages are transmitted and received through an externally connected USB host.

  • Installation notes:

    • You can use a single EnOcean gateway connected to the USB port on the top of the controller case.

    • If needed, the gateway can be extended using an extension cable (up to a maximum of 5 meters).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?