250929_LSS100100/LSS100200_SW_03.0

Touch Configuration

When setting up your Touch visualization, keep the following points in mind:

  1. Visualization structure:

    • Your visualization can include multiple floors and rooms.

    • Think of it as a hierarchical structure that represents your building or home layout.

  2. Rooms and widgets:

    • Within each room, you have options:

      • Pre-made widgets: Use ready-made widgets to quickly populate your rooms with essential automation controls.

      • Custom widgets: Create your own widgets using the Widget creator tool.

  3. Position display:

    • As you build your structure, the current position is shown at the bottom center of the screen.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?