250929_LSS100100/LSS100200_SW_03.0

HomeKit Plugin

The HomeKit plugin for Wiser for KNX/spaceLYnk controller is designed to control KNX devices in the installation through Apple´s Home application, available in Apple devices like iPhone, iPad, iWatch, Mac, Apple TV, etc. (hereafter referred to as the app/mobile application).

System Requirements

To ensure optimal performance and compatibility with HomeKit plugin, please make sure you meet the following system requirements:

Hardware

Wiser for KNX or spaceLYnk controller

Ensure you have a hardware version greater than 2.

Firmware

Latest firmware

Make sure you have the latest firmware installed.

The latest firmware is available for download at se.com.

Software

Plugin

Ensure the KNX IoT 3rd Party API plugin is installed and enabled (for Local).

Enabling automatic updates is recommended to ensure you always have the latest version of the plugin installed.

Limitations of the HomeKit plugin:

  • Control of slats in blinds (not supported).

  • Stop commands for shutters/blinds.
  • Heating works only in the room temperature controller.
  • KNX scenes cannot be called, but new scenes can be created in the Home app.

  • Separate settings from the Touch plugin.

  • Terminology/naming of group objects is different from KNX conventions.

  • In larger or more complex KNX installations, the app may behave unreliably.

Home app

The Home app can be operated in two ways:

  1. Without a home hub: You can control the KNX installation locally from your mobile device using the HomeKit plugin.

  2. With a home hub (e.g., Apple TV): With a home hub, you can access the installation remotely via the internet through Apple Cloud. Additionally, you can set up automations/scenes and share your home with other users.


Main features of the Apple Home app

The Home app is a centralized hub to control and manage your smart home devices. Here are the key features:

  1. Device control: You can manage a variety of smart devices such as lights, thermostats, cameras, and locks directly from the app. Toggle devices on or off and adjust settings to suit your preferences.

  2. Scenes: Create customized scenes that allow you to control multiple devices simultaneously.

  3. Automations: You can set up automations to trigger actions based on specific conditions such as time of day, location, or device activity.

  4. Secure remote access: Access and control your devices remotely through an Apple TV or HomePod acting as a hub. This ensures you can monitor and manage your home even when you're away.

  5. User sharing: Share control of your devices with family members and friends, allowing them to access and manage devices from their own Apple devices.

  6. Room and zone management: Organize your smart home devices by assigning them to specific rooms and zones within the app.

For more information about the Apple Home app, visit https://www.apple.com/uk/home-app/.

You can find the user guide for the Apple Home app at https://support.apple.com/.



Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.