ETS 4
To utilize the controller with KNX TP UART/IP functionality and program other KNX bus devices, follow these steps to add the controller to the ETS Connection manager.
ETS programming through the controller is available only when KNX IP features are enabled.
-
Navigate to Settings > Communication.
-
Newly added controller will be automatically discovered if it is connected to the same network as the PC running ETS 4 software.
-
Choose Select to move it to the Configured connections.
-
Set the controller KNX individual address and mask by clicking Local settings.
-
Select the Use project connection if available checkbox to make it the default project connection.
-
If direct communication in the IP network is desired, select the Use direct KNX-IP connection if available option.
-
Click New to manually add the controller and enter any name for the device.
-
Set the IP address, Port, and NAT mode (if needed).
-
Click OK to save the changes.
-
To test communication with ETS, click Test.
-
Finally, click Apply changes for the changes to take effect.