Modbus Settings in the Controller Using Device Profiles
All Modbus communication settings for the controller are accessible through the Modbus tab. Device profiles play a crucial role in mapping Modbus addresses (registers) to KNX group objects. If you need to read or write a Modbus register, simply configure the mapping rules, allowing you to access the register via KNX group objects.
Here is a step-by-step guide for Modbus communication settings:
-
Modbus RTU configuration:
-
Specify the details for Modbus RTU communication, such as baud rate and parity.
-
This step applies if you’re using Modbus RTU.
-
-
Device profile upload:
-
Ensure that a device profile is uploaded in the controller.
-
Preinstalled profiles for Schneider-Electric devices are available, and you can also upload custom Modbus profiles.
-
-
Add the device:
-
Add your Modbus device to the device list.
-
-
Register mapping:
-
Configure the mapping between Modbus registers and KNX group objects.
-
-
Automatic discovery:
-
To find Modbus devices connected to the controller via Modbus RTU, use the scan function.
-
Access it here: Configurator → Modbus → RTU scan.
-
Devices marked as RTU scan = No do not support automatic discovery.
-
|
Modbus device |
RTU scan |
Modbus device |
RTU scan |
Modbus device |
RTU scan |
|---|---|---|---|---|---|
|
Compact_NSX-Compact_NSX_E |
No |
PM-PM820 |
No |
EM-EM6400 |
- |
|
Masterpact_NT_NW-Masterpact_A |
No |
PM-PM850 |
No |
EM-EM6433 |
- |
|
Masterpact_NT_NW-Masterpact_H |
No |
PM-PM870 |
No |
EM-EM6434 |
- |
|
Masterpact_NT_NW-Masterpact_P |
No |
PM-PM9C |
No |
EM-EM6436 |
- |
|
PM-PM1200 |
No |
SIM10M |
No |
EM-EM6436 and EM-EM6436dual |
- |
|
PM-PM210 |
No |
Smartlink-RTU |
Yes |
EM-EM6438 |
- |
|
PM-PM3250 |
Yes |
Smartlink-TCP |
No |
ION-ION6200 |
- |
|
PM-PM3255 |
Yes |
SE8300 |
No |
ION-ION7300 |
- |
|
PM-PM5110 |
No |
SE8600 |
No |
ION-ION7330 |
- |
|
PM-PM5111 |
No |
SER8300 |
No |
ION-ION7350 |
- |
|
PM-PM5310 |
No |
TC303 |
No |
ION-ION7550 |
- |
|
PM-PM5330 |
No |
iEM-iEM2150 |
Yes |
ION-ION7650 |
- |
|
PM-PM5350 |
No |
iEM-iEM2155 |
Yes |
Masterpact_NT_NW-Masterpact_E |
- |
|
iEM-iEM3150 |
Yes |
Vigilohm IM20 |
Yes |
PM-PM500 |
- |
|
iEM-iEM3155 |
Yes |
Vigilohm IM400 |
Yes |
PM-PM5111 |
- |
|
iEM-iEM3250 |
Yes |
PowerTag |
No |
PM-PM5320 |
- |
|
iEM-iEM3255 |
Yes |
CM-CM3250 |
- |
PM-PM5331 |
- |
|
iEM-iEM3350 |
Yes |
CM-CM3350 |
- |
PM-PM5340 |
- |
|
iEM-iEM3355 |
Yes |
CM-CM4000 |
- |
PM-PM5341 |
- |
|
PM-PM710 |
No |
Compact_NSX-Compact_NSX_A |
- |
PM-PM5560 |
- |
|
PM-PM750 |
No |
EM-EM3550 |
- |
PM-PM5561 |
- |
|
PM-PM810 |
No |
EM-EM3555 |
- |
PM-PM5563 |
- |