250929_LSS100100/LSS100200_SW_03.0

New Features – FW Version 3.0.0

A full list of new features with descriptions is available in the changelog.

Feature

Link to the chapter

KNX data secured group address feature

Add New Object: KNX data secure key

Read-only trends

Trend Logs

IP settings in KNX connections

KNX Connection

802.1X EAP TLS network setting added

802.1X EAP–TLS

User detail - new feature - Home page setting

Add New User

Acceptance of the NTP server from DHCP server

Interfaces
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?