250929_LSS100100/LSS100200_SW_03.0

Editing and Deleting Devices in HomeKit Plugin

You can later edit/delete the devices mapped in the HomeKit plugin:


  1. Editing devices:

    • Click on the right of your device's row.

    • Make the intended changes.

    • Click on Save and then Apply changes to save the updates.


  2. Deleting devices:

    • Click on the right of your device's row.

    • In the Delete device dialog, click on Delete.

    • Remember to click on Apply changes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?