250929_LSS100100/LSS100200_SW_03.0

Blinds and Dimming with EnOcean

The controller now includes a new EnOcean feature implemented since firmware version 2.5.0. This feature enables the controller to handle dimming and blind functions while recognizing the long and short presses of EnOcean pushbuttons. Specifically, it applies to EnOcean profiles F06-03-02 and F06-03-03.

Here’s how it works:

  1. Mapping EnOcean Pushbuttons:

    • When mapping EnOcean pushbuttons, you will open a settings dialog that allows you to configure short and long press settings.

  2. Short press modes:

    • Choose from the following short press modes:

      • On/Start/Down/Close

      • Off/Stop/Up/Open

      • Toggle

      • Start/Stop

      • Stop/Start

      • Scene

    • Short press object: Additionally, link a KNX object to the short press action.

  3. Long press modes:

    • Long press modes include:

      • No Action (disabled)

      • On/Start/Down/Close

      • Off/Stop/Up/Open

      • Toggle

      • Dimming up

      • Dimming down

    • Long press object: Link a KNX object to the long press action.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?