250929_LSS100100/LSS100200_SW_03.0

System Status

The system information is displayed in the following tabs:

  1. General: Provides details about the hardware and system, as provided by the kernel.

  2. Memory usage: Shows the current memory utilization by the system.

  3. Partitions: Lists the available partitions in the system.

  4. Serial ports: Displays the list of available serial ports.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?