250929_LSS100100/LSS100200_SW_03.0

Object Logs

In the Object logs tab, you can access historical telegrams for objects. Once logging is enabled for an object, all future data will be logged.

Filtering options are available when you need to find specific information within a period:

  1. Start date: Specify the start date and time for log filtering.

  2. End date: Specify the end date and time for log filtering.

  3. Name or group address: Filter by a specific name or group address of the object.

  4. Tags: Group objects with the same tags.

  5. Value: Filter by a specific object value.

  6. Source address: Filter by a specific source address.

You can clear all logs by clicking the Clear button.

To configure logging memory properties, navigate to UtilitiesGeneral configuration.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?