250929_LSS100100/LSS100200_SW_03.0

Web Server Software NGINX

NGINX, the web server software used for the controller, offers improved performance with minimal memory usage. Find more information at https://www.nginx.com.

If you are using pre-1.2 versions of firmware, remember to clear your browser cache after a firmware upgrade. Additionally, be aware that Nginx uses different links to pages compared to older versions:

  • Main page link (old versions):

    • Example: http://your_IP_address/cgi-bin/scada-vis/index.cgi

  • Main page link (NGINX):

    • Example: http://your_IP_address/scada-vis

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?