EnOcean → KNX Mapping
EnOcean devices transmit telegrams periodically. When an EnOcean gateway receives a telegram, the corresponding device appears in the Configurator → EnOcean → EnOcean >> KNX section.
Most EnOcean devices include a dedicated button that allows immediate telegram transmission without waiting for periodic intervals.
To map a specific EnOcean device to KNX, follow these steps:
-
Click the corresponding row for the device in the list.
-
Specify the EnOcean Profile for the device.
-
Optionally, assign a device name.
-
Click Save.
-
All supported device profiles are listed in the Supported EnOcean Profiles section.
Once the device profile is specified, you can proceed with mapping to KNX objects:
-
Click
on the desired line in the device list to open the Device
mapping dialog. -
Each data object from the EnOcean device can be linked to a KNX object in the controller.
-
Select the appropriate controller object from the drop-down menu or create a new object directly from the dialog using the
icon. -
If the Write to bus parameter is enabled, the value is sent to the KNX TP bus.
When the EnOcean gateway receives a telegram from a specific device, the corresponding row is highlighted in green, and the respective KNX group address is updated with the new value from EnOcean.