250929_LSS100100/LSS100200_SW_03.0

ARP Table

The Address Resolution Protocol (ARP) table can be found under the NetworkARP table.


Its primary function is to resolve network layer addresses into link layer addresses.

In simpler terms, it transforms an IP address into a corresponding physical address.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?