250929_LSS100100/LSS100200_SW_03.0

The VPN Access

The VPN access (VPN = Virtual Private Network) authorises the portable device to access the local network and, therefore, the KNX installation via the Internet.


Benefits of VPN

  • Only authorised users have access to the local network.

  • All data is encrypted.

  • The data is not changed, recorded or diverted during the transfer (often referred to as a VPN tunnel).


Requirements for setting up a VPN connection

  • Internet connection.

  • The portable device and the router are enabled for a VPN connection (VPN client installed).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?