Automations
Automations allow you to create customized sequences and actions for your devices, enhancing convenience and efficiency. By setting up automations, you can ensure that your devices respond to specific conditions or schedules without manual intervention.
Automations trigger devices automatically when specific conditions are met. For example:
-
If it is sunrise, open my living room blinds.
-
If motion is detected on weekends between 9:00 and 17:00, do not switch on the lights.
You need to install the Automation plugin to utilize automation with your controller. This plugin is available in the controller's Marketplace.
Follow these steps to install the Automation plugin:
-
Click
on the Start page of your controller to open the Marketplace.
-
Switch to the Install new apps and widgets section.
-
Enter the “Automation” in the search field.
-
After you find the plugin, enable automatic updates for it.
Once the plugin is installed, you can start creating and managing
automations directly in the controller’s Configurator, in the Automations tab.