250929_LSS100100/LSS100200_SW_03.0

Visualization Map

  • When adding a new object, it will be placed in the top-left corner of the plan, following the predefined vertical and horizontal spacing from the object menu.

  • The selected object can be resized by dragging the strip on the bottom or right side. You can also delete or duplicate it (the duplicated object will maintain the predefined spacing).

  • To enable the snap-to-grid feature, click next to the element position in the Plan editor.

  • The Copy button allows you to copy existing visualization objects from one plan to another.

  • The Paste button becomes available when a visualization object has been selected for copying.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?