250929_LSS100100/LSS100200_SW_03.0

Read Test

This feature allows for a quick test of RTU communication. To initiate the RTU read test, follow these steps:

  1. Click the Read test button in the Modbus tab.

  2. Set up the parameters in the Read test dialog as follows:

    • Device address: Specify the address of the Modbus device.

    • Function: Choose between Coil, Discrete input, Holding register, and Input register functions.

    • Address: Enter the register address.

    • Data type: Select the appropriate message data point type.

    • Read swap: Adjust the order of reading if needed.

    • Read length: Define the length of the read message.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?