250929_LSS100100/LSS100200_SW_03.0

EnOcean

EnOcean is an energy-harvesting wireless technology that enables communication between devices such as push buttons, thermostats, and PIR sensors within the controller ecosystem. By integrating EnOcean, the controller expands the possibilities of wired KNX installations, offering easy implementation and configuration.

To enable EnOcean technology in the controller, you will need to connect a USB EnOcean gateway (EnOcean USB Gateway).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?