2410_LSS100100/LSS100200_SW_03.0

KNX Data Secure

If you have data secure devices in your KNX installation and need your controller to communicate directly with these devices (sending and receiving data secure telegrams), follow these steps:

  1. Add the controller secure dummy device:

    • Integrate the controller secure dummy device into your KNX installation.

    • You can use the SpaceLogic KNX Secure Dummy device provided by Schneider Electric available in the ETS catalogue.

    • Connect the individual group addresses of the data secure device to your controller dummy device.

  2. Controller as a router:

    • If your controller functions as a router (facilitating communication between KNX devices), you do not need the controller secure dummy device for secured KNX communication.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?