250929_LSS100100/LSS100200_SW_03.0

Object

The Object tab allows you to configure control and monitoring settings for various objects. Different data types have distinct parameters:

  1. Main object:

    • Displays existing group addresses on the KNX/EIB bus available for configuration in the Objects tab.

    • To speed up selection, consider typing group addresses directly.

  2. Visualization parameters:

    • Adjust object visualization parameters

      • Control type: Choose the appropriate control type.

      • Minimum/Maximum value: Set the range for the parameter.

      • Step: Define the increment value.

      • Colors and size: Customize visual aspects.

    • After clicking the Visualization parameters button, choose one of the following options in the Select which parameters to edit dialog:

      • Global (per object) parameters: These settings apply to all visualization elements with the same object.

      • Local (per-element) parameters: Customize settings for specific visualization elements.

      • Override global parameters with local: Modify the object based on local settings.

      • Clear local parameters: Reset local customizations.

  3. Status object:

    • Lists status objects on the KNX/EIB bus.

    • Control objects can also serve as status indicators.

  4. Custom name:

    • Assigns a name to the object.

    • Important for Smartphone Visualization; if left blank, the group address name is used.

  5. Read-only:

    • Makes the object read-only, without write (control) permission.

  6. Hide in Smartphone:

    • Prevents the object from appearing in smartphone visualization.

  7. Hide background:

    • Hides the icon background.

  8. Send fixed value:

    • Allows sending a specific value to the bus when the object is pressed.

  9. No bus write:

    • Prevents writing the value to the KNX bus.

    • Useful for triggering scripts with busload limitations.

  10. Pin code:

    • Adds PIN protection to the object.

    • Requires entering a PIN when changing the value.

    • Minimum PIN length: 4 digits with brute force protection.

  11. Widget:

    • Attaches a widget to a button (requires prior creation).

    • Widget testing available only in PC/tablet visualization.

  12. Display mode:

    • Determines how the object is displayed.

  13. Smartphone icon:

    • Default icon for smartphones (can differ from PC/tablet icon).

  14. Additional classes:

    • Creates custom CSS classes to modify graphical objects.

  15. Font size:

    • Defines display text style for values.

  16. Text styles:

    • Options for bold, italic, and underscore.

  17. Custom font:

    • Choose from installed fonts.

  18. Show value background:

    • Enhances readability by showing value backgrounds.

  19. Show control:

    • If enabled, control button graphics change from symbols to switches (visible in PC/tablet visualization).

  20. Additional icons (for value-type objects):

    • Specify additional icons while setting parameters.

You can adjust these parameters to customize your object behavior.

After defining the parameters, click Add to plan to create a new object.

Cancel button sets the object parameters to default settings.

Objects can be moved within the plan, duplicated, and edited.

Element position:

  • You can add elements manually or by dragging and dropping objects to set their X and Y axis positions on the plan.

Element size:

  • Adjust the element size manually or by dragging a vertical-horizontal strip of the object.

  • The minimum value for size is 5 × 5 pixels.

  • To reset an object size to the default, click .

  • Lock the aspect ratio of the object by clicking .

When ready, click Save and reload plan to activate the objects.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?