250929_LSS100100/LSS100200_SW_03.0

Gauge

The Gauge tab enables dynamic visualization and allows you to change the object value displayed in the gauge. Follow these steps to set up the gauge parameters:

  1. Data object:

    • Specify the KNX group address associated with the gauge.

  2. Gauge size:

    • Define the desired dimensions for the gauge.

  3. Custom name:

    • Provide a custom name for the gauge object.

  4. Read-only:

    • Toggle this option to make the gauge read-only (if needed).

  5. Additional classes:

    • Create an additional class for custom CSS modifications targeting specific graphical objects.

Once you have defined the gauge parameters, click the Add to plan button. A newly created object will appear on the map, which you can move to your desired location.

Adjust the element size and position (refer to Object).

Click Save and reload plan to activate the gauge.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?