250929_LSS100100/LSS100200_SW_03.0

System: Quick Menu

By clicking the arrow located on the right, you will open a menu that contains the system settings most frequently used.

KNX Connection

KNX Connection

Network Settings

Interfaces

Admin Access

Admin Access

Remote Services

Remote Services

Toggle Device Identification

By selecting the Toggle Device Identification option, you will activate a red/green flashing sequence on LED 2 of the device.

This feature is designed to assist in the easy identification of the controller within the cabinet.

Remote Connectivity

Remote connectivity allows you to connect to the controller remotely via a web browser.

By default, remote connectivity is disabled for the spaceLYnk controller.

By default, remote connectivity is enabled for the Wiser for KXN controller.


Prerequisites:

For the controller

For the user

Ensure port 80 is open with the OpenVPN service running.

Allow ports 80 and 443 for HTTP and HTTPS communication.

Once the prerequisites are fulfilled, remote connectivity will be possible, allowing you to access the controller remotely via your web browser.


Remote connectivity via WireGuard is necessary in order to change KNX device settings through eConfigure or to perform their commissioning.

Prerequisites:

For the controller

For the user

Ensure port 51820 is open with the WireGuard service running.

Ensure port 51820 is open.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?