250929_LSS100100/LSS100200_SW_03.0

Resident Script

A resident script is a script that runs directly on the controller itself. To set up a resident script, follow these steps:

  1. Click the Resident button in the Scripting tab.

  2. Click the Add new script button.

  3. Configure the parameters in the Resident script dialog as follows:

    • Script name: Specify a descriptive name for the script.

    • Sleep interval (seconds): Set the interval after which the script will execute.

    • Active: Choose whether the script is active (green circle) or disabled (red circle).

    • Category: Assign a new or existing category name to group similar scripts (this will not affect the script’s action but helps with organization).

    • Description: Provide a brief description of the script.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?