250929_LSS100100/LSS100200_SW_03.0

Set Object Value

To change the object value, follow these steps:

  1. Click corresponding to your object in the object list.

  2. In the New value field of the Set object value dialog, type the desired value for your object.

  3. Click Save to confirm the change.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?