250929_LSS100100/LSS100200_SW_03.0

Marketplace

This icon navigates to the Marketplace page. It is available only in admin mode. If there is no internet connection, only installed applications will be visible, and updates won’t be possible.

The icon on the left side opens the following sub-menu:

  1. Apps: Displays all available applications.

  2. Installed: Shows all installed applications (the yellow number indicates the count of installed applications).

  3. Install from file: Installs an application directly from a file.

Search bar

Filters applications based on typed letters.

Installs the selected application.

Updates the selected application.

Uninstalls the selected application.

Marks applications verified by Schneider Electric. Applications not verified are not officially supported by Schneider Electric, and their use is at your own risk.

Applications signing:

  • Applications installed from a file should be verified by signature, similar to all applications on the Marketplace.

  • Installation of applications without a signature is still possible, but ensure that you trust the source and specifically select this option in a dialog window.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?