250929_LSS100100/LSS100200_SW_03.0

Object Visualization Priority

In the context of visualization, each object has a specific priority. Below, the objects are listed from highest to lowest:

  1. Text label on plan

  2. Object on plan

  3. Plan link as text on plan

  4. Plan link as icon on plan

  5. Camera on plan

  6. Graph on plan

  7. Gauge on plan

  8. Image on plan

  9. Frame on plan

  10. Text label on layout

  11. Object on layout

  12. Plan link as text on layout

  13. Plan link as icon on layout

  14. Camera on layout

  15. Graph on layout

  16. Gauge on layout

  17. Image on layout

  18. Frame on layout

  19. Background of plan

  20. Background of layout

Keep in mind that the order of objects with the same priority is not explicitly defined and may vary between the editor and PC/tablet visualizations.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?