250929_LSS100100/LSS100200_SW_03.0

Object Filter

On the left side of the object list, you can filter objects based on the following values:

  1. Name or group address: Filter by name or group address. You can use * to replace digits in the address for range filtering.

  2. Data type: Filter by the data type of objects.

  3. Tags: Filter by tags. You can choose between matching all tags or any tag.

Click the Apply filter button for the filter to take effect.


Mass edit

Objects filtered in the object filter can be mass-edited in the following ways:

  1. Object properties: Mass edit based on object properties as listed in the objects menu.

  2. Visualization parameters: Mass edit based on visualization parameters (e.g., toggle, checkbox, slider).

  3. Custom values: Mass edit based on custom values for boolean and integer data types.


Mass delete

Objects filtered in the object filter can be mass-deleted using the following options:

  1. Delete unnamed objects: Delete all unnamed objects from the list.

  2. Delete objects from current filter: Delete all objects selected by the current filter.

  3. Wildcard search in objects: Filter on all objects with a search string (e.g., “*.G*_S”).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?