250929_LSS100100/LSS100200_SW_03.0

Custom Values

To add custom text to object values, follow these steps:

  1. Click in the object list.

  2. In the Custom value dialog, click Add custom value, type the object value, and define the custom text. Then click Save.

  3. To delete an object value, click corresponding to your value in the Custom value dialog.

The Default text will be displayed if the value is not defined.

NOTE: Custom text values can only be set for boolean or integer values. You can filter objects based on the Custom values (Object Filter).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?