250929_LSS100100/LSS100200_SW_03.0

BACnet COV Settings

When exporting objects to BACnet, they can be subscribed by the BACnet client using Change of value (COV) subscriptions.

To find all analog values active for COV subscription, navigate to:

ConfiguratorUtilitiesSystemNetworkBACnet COV settings.


Each analog value that is active for COV subscription has a parameter called COV increment. This parameter defines the minimal change of value (delta) that triggers a value update on the client side. By default, the COV increment is set to 1. This means that unless the value in the controller changes by more than 1, the client-side value remains unchanged.


If you modify the COV increment parameters in ConfiguratorUtilitiesSystemNetworkBACnet COV settings and save the changes, all existing COV subscriptions will be canceled. To resume COV subscriptions, they must be restarted from the client side.


IMPORTANT: Changing COV increment values also resets the priority array values of all objects.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?