250929_LSS100100/LSS100200_SW_03.0

Graph

The Graph tab allows you to integrate real-time graphs into a visualization system for monitoring scale-type objects current and historical values. Follow these steps to set up the graph parameters:

  1. Data object:

    • Specify the group address of the object.

    • Ensure that the object has the Log option activated for the graph to function in visualization.

  2. Custom name:

    • Assign a name to the object.

  3. Icon:

    • Choose an icon to launch the graph.

  4. Window size:

    • Define the width and height for displaying the graph.

  5. Number of points:

    • Determine the maximum number of data points to display in the graph (up to 200 points).

  6. Auto-follow value:

    • Use this option for objects that never reach zero value (e.g., CO2 levels). It improves graph resolution.

  7. Auto open window:

    • The graph window automatically opens when accessed.

  8. Hide background:

    • Choose whether to hide the icon background.

  9. Additional classes:

    • Create an additional class for custom CSS modifications targeting specific graphical objects.

Once you have defined the graph parameters, click the Add to plan button, and a newly created object will appear. You can move this object to your desired location.

Adjust the element size and position (refer to Object).

Click Save and reload plan to activate the objects (with a delay for obtaining relevant data).

IMPORTANT: Ensure that the object providing data is set as logged in its properties (see Add New Object).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?