250929_LSS100100/LSS100200_SW_03.0

Reboot

The Reboot feature of the controller allows users to safely restart the device without interrupting system integrity or requiring a manual power cycle.

This function is useful when applying configuration changes, resolving minor system issues, or refreshing the controller’s operation.

To initiate a reboot:

  1. Open the Configurator.

  2. Navigate to System > System.

  3. Select Reboot and confirm by clicking OK.

The controller will then restart automatically, temporarily becoming unresponsive during the process. This ensures a clean reboot while preserving all saved settings and configurations.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?