250929_LSS100100/LSS100200_SW_03.0

Start-Up (Init) Script

The initialization script (init script) is used to set up specific system or bus values when the system starts. This script runs each time after the system has restarted, whether due to power-up, software reboot, or via a hardware reset push button.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?