250929_LSS100100/LSS100200_SW_03.0

Adding Accessory to the Home App via QR Code

After mapping the devices in the HomeKit plugin, transfer them to the Home app using a bridge created by the mobile app. This bridge represents the controller. To complete the transfer, use the QR code generated by the HomeKit plugin.


Follow these steps:

  1. Make sure that your mobile device and HomeKit plugin are connected to the internet on the same network.

  2. In the HomeKit plugin, on the main screen, click on the QR code button at the top right. A Setup code dialog will open with a generated QR code for pairing.

  3. Open the mobile application on your mobile device, and tap Add Accessory.

  4. Point your mobile device at the QR code in the HomeKit plugin.

  5. The mobile app will load a bridge from your HomeKit plugin. You can then name your devices using the wizard and assign them to individual rooms in the mobile app.



NOTE: The Apple Home app supports adding multiple bridges, allowing you to integrate other Apple HomeKit-compatible systems and devices, such as cameras and sensors.
Additionally, the Apple Home app enables you to create automations and scenes that combine all the devices integrated into the Home app.
For more information, please refer to the Apple HomeKit user guide.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?