250929_LSS100100/LSS100200_SW_03.0

Patch Management

Effective patch management is crucial for maintaining the security and performance of your systems. Here are some essential guidelines:

  1. Install updates:

    • Refer to Install Updates to install patches and firmware add-ons.

    • Always perform upgrades manually.

  2. Backup before upgrading:

    • Backup outlines the backup procedure.

    • Prior to any upgrade, ensure you have a reliable backup.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?