250929_LSS100100/LSS100200_SW_03.0

Access Logs

Click the Access logs button in the User access tab to view login history.

Unsuccessful logins are marked in red, and FTP and applications access are also logged.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?