250929_LSS100100/LSS100200_SW_03.0

Start Page Configuration

  1. Configuration

    • Click this icon to navigate to the Configurator page.

    • Select the language for the user interface.

    • Choose between light/dark theme of the interface.

    • Unlock the menu for editing by clicking . The menu will turn light red (admin mode only).

    • Click and click to:

      • Allow users to show/hide applications on the main screen. Users can modify the visibility of icons on the main screen (when permitted by the admin).

        This feature is available only in admin mode.
      • Change admin password: This option is available only when in admin mode.

  2. Search

    • Filter menu applications based on typed letters.

  3. Lock / unlock grid

    • Lock or unlock the grid to sort the order of icons in the menu.

  4. Show / hide applications:

    • Allows showing or hiding applications on the main screen. This feature is available in admin mode or user view (when permitted by the admin).

  5. Save view : Save the default view of the user’s home page.

  6. Controller mode

    • If the controller is in admin mode, clicking will log off.

    • If the controller is in user mode, clicking will also log off.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?