Layouts
A layout serves as an advanced background for plans. You can place any object from the editor onto the layout, which can then be attached to one or multiple plans. While all objects from the layout will be visible on the plan, the objects on the plan will appear above those from the layout.
To add a layout, follow these steps:
-
Click
in the Layouts/Widgets tab → click Add or use the Add new layout button at the bottom left of the tab. -
Fill in the Layout dialog with the following details:
-
Name: Provide a name for the layout.
-
Plan size: Choose the size of the layout (pre-defined sizes are available in the drop-down menu).
-
Primary background image: Select the primary background for the layout.
-
Secondary background image: Choose the secondary background for a parallax effect. Use a background previously added to Vis. graphics → Images/Backgrounds.
-
Background color: Pick the background color for the layout.
-
Smartphone background color: Choose the background color for smartphone visualization.
-
Repeat background image: Decide whether to show the image once or repeat it to fill the entire layout.
-
Fixed primary background: Use a static primary picture for Parallax projection.
-
-
Click Save.
Your new layout will appear in the Layouts/Widgets tab. You can further edit it, duplicate it along with all its components, change its sort order, export or delete it.
Remember that the content of this layout should be defined under the Visualization tab.