250929_LSS100100/LSS100200_SW_03.0

Connectivity

  • IP LAN connection 10/100 Mbit

  • USB 2.0 (for GMS modem, EnOcean…) 5V, 500 mA max.

  • RS-232

  • Modbus (RS-485)

  • Wi-Fi through IP connection and wireless router

  • KNX/EIB TP Bus

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?