250929_LSS100100/LSS100200_SW_03.0

Objects

The list of KNX network objects appears under ConfiguratorObjects.

Objects are categorized as follows:

  1. Captured by sniffing the bus:

    • If enabled in Utilities, objects are captured by sniffing telegrams from unknown group addresses.

  2. Manually added:

    • Objects added manually.

  3. Imported from ESF File:

    • Objects imported via the ESF file in Utilities.


Objects are sorted based on the following parameters:

  • Group address

  • Object name

  • Event script

  • Data type

  • Current value

  • Log and export settings

  • Tags

  • Last update timestamp

  • Set value

  • Visualization parameters

  • Custom values


Additionally, objects are visually distinguished by background color:

  • Yellow: Object discovered by a bus sniffer.

  • Green: Object value has been updated.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?