250929_LSS100100/LSS100200_SW_03.0

Remote Diagnostics

You have the option to enable or disable remote diagnostics. To do so, follow these steps:

  1. Port forwarding: Ensure that port 22 is forwarded on your router.

  2. Enable Service status.

  3. Click OK.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?