250929_LSS100100/LSS100200_SW_03.0

Scheduler → Events

Scheduler events can be added either in the administrator interface or by users in the special user mode Schedulers interface.

Follow these steps:

  1. Click to open the Events list.

  2. Click Add Event and fill in the Event dialog with the following details:

    • Active: Define whether the event is active or not.

    • Name: Provide a name for the event.

    • Run at: Specify whether the event will be triggered by a specific time, sunrise, or sunset.

    • Start time offset: Set an offset for sunrise/sunset (useful for locations in valleys or surrounded by hills).

    • Start time: Specify the time of event activation.

    • Day of the week: Choose the days on which the event will be active.

    • Weekday in month: Select the weekday (e.g., first Monday) for the event (which may fall in the second week of some months).

    • Months: Specify the months in which the event will be active.

    • Year: Optionally, set a specific year for the event (leave blank for recurring events).

    • Holidays: Define the behavior during holidays (options include No effect, Do not run on holidays, and Run only on holidays).

    • Value: Determine the value to send to the group address when the event is triggered.

  3. Click Save.

NOTE: It is recommended that administrators create all necessary schedulers, as users can only add events but not full schedulers.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?