250929_LSS100100/LSS100200_SW_03.0

Adding New Scene

  1. Click the Add Scene button to create a new scene.

  2. Fill in the Scene dialog with the following details:

    • Name: Specify the name for your scene.

    • Scene is active: Toggle this option to enable or disable the scene.

    • Trigger object: Choose the object that activates the scene.

    • Trigger value: Set the value of the object that triggers the scene.

    • Tags: Add scene tags (only applicable if the scene is not compatible with object tags).

  3. Click Save. Your new scene will now appear in the list of scenes, where you can edit, duplicate, or delete it.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?