250929_LSS100100/LSS100200_SW_03.0

Import ESF File

Use the Import ESF File button to import your *.esf object files.

It is crucial to assign the correct data types to the objects you are importing.

NOTE: Existing objects will not be overwritten.

Objects that share the same name are treated as duplicates and may not be imported. These objects will be marked as discarded.

To import *.esf files, follow these steps:

  1. In the Utilities tab, click the Import ESF File button.

  2. Select the file you wish to import.

  3. Click OpenSave.

After each import, a list of both imported and discarded objects will be displayed in the Import Result dialog window.

Comments related to ETS imports will be displayed in the Object comments section for each imported ETS object:

Objects tab → find your object → click it → see the comments.

For more details, please refer to chapter Import KNX Project from ETS.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?