250929_LSS100100/LSS100200_SW_03.0

Differences between spaceLYnk and Wiser for KNX

Feature

Wiser for KNX

spaceLYnk

Modbus GUI

Up to 10 Modbus devices

Up to Modbus addressable range ≥ 31 by default

BACnet Server

Up to 150 exported objects

*No limit (≤ 2000 recommended)

User Administration

Up to 8 users

No limit (≤ 20 recommended)

One click adding to the filter table (object filtering)

N/A

Fully supported

*Performance testing was measured on HW3.0 when the object value change interval was set to 60 s. The recommended limit for HW1.x remains 500 objects.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.