250929_LSS100100/LSS100200_SW_03.0

Create Automation

Add Automation

To add new automation, follow these steps:

  1. Click the Add automation button at the bottom left of the Automations tab.

  2. Fill in the Automation dialog as follows:

    • Active: Select whether you want to activate your automation immediately.

    • Name: Provide a descriptive name for your automation.

    • Conjunction: Choose the logical conjunction for automation conditions:

      • AND: All conditions must be fulfilled to trigger an automation.

      • OR: Any condition will trigger an automation.

    • Status object: Choose a status indication object.

    • Status value true: Specify the Status object value for the automation conditions evaluated as true.

    • Status value false: Specify the Status object value for the automation conditions evaluated as false.

  3. Click Save.

Condition

In the next step, you will define the conditions for your automation. A condition is a specific criterion that must be met for an automation to be triggered.

For example: If the level of CO2 exceeds 1000 ppm.

You can compare objects and/or values:

  1. Click in the Conditions column of your automation

  2. Click Add condition.

  3. Fill in the Condition dialog and click Save.

NOTE: Either Value to compare or Object to compare must be set. When both are set, Object to compare takes precedence, and Value to compare is ignored.

Scenes

You can associate a scene with your automation. When the specified conditions are met, the scene will be triggered.

  1. Click in the Scenes column of your automation

  2. Click Add scene.

  3. Select your scene and click Save.

Events

You can assign an Event to your automation. Events can be scheduled to occur at certain times.

For example, you can set an event to turn on the lights at sunset.

Follow these steps to set up an Event:

  1. Click in the Events column of your automation.

  2. In the dialog box, choose when you want your automation to trigger. You have three options:

    • Sunset

    • Sunrise

    • A Specific time that you set

  3. Select the days of the week when the automation should run.

  4. Click Save.

NOTE: If you do not set up Events, the automation will trigger whenever the conditions are met.

Intervals

Intervals refer to the specific time durations of actions.

For example, you can set an automation to water the garden for 30 minutes every morning at 7 AM.

Setting up Intervals is similar to setting up Events. In the dialog box, choose the start and end times of the interval and select the day on which the automation should be executed within the specified interval.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?